ALTERNATIVE

pLEASE CONFIRM IF P/N SMF13A AND SMF13A-T13 ARE SAME AND CAN I USE SMF13A
AS AN ALTERNATIVE AND WHAT DOES T13 MEAN

Hello @malavb

Yes, part number SMF13A and part number SMF13A-T13 are the same part, and the difference is in the size of the reels they come on. The SMF13A comes on a 7" reel with 3000 Tvs diodes to a reel. Whereas the SMF13A-T13 comes on a 13" reel with 10,000 Tvs diodes to a reel. We do sell both of these parts in individual quantities so you can buy just 1 Tvs diode if you would like.

The ‘T13’ is calling out the change in reel size from the smaller 7" reel to the bigger 13" reel.