What is Aoyue Mod?
Do the soldering tweezers plug into wall socket or into a station?
What temperature in Celsius degrees do the soldering tweezers reach?
Does the AON-1305 Flat Tip attach to AOT004?
Hello peterho,
Thank you for contacting the TechForum.
In regards to your questions, The Aoyue Mod is referring to the Series Aoyue from SRA Soldering Products.
The AOT004 Soldering Tweezers will Plug into a Station Not a wall socket.
The Stations that will work with the AOT004 are AO701A++ and AO968A+
The AO701A++ will have a Temp range of 392°F ~ 896°F (200°C ~ 480°C) so that will be the Temp range for the AOT004 Tweezer. So with that the Max temp will be the 480°C.
The AO968A+ will have a Temp Range of 212°F ~ 896°F (100°C ~ 480°C). The Max temp will be the same.
Yes the AON-1305 Flat Tip will work on the AOT004
If you have any questions Please let is know.
Thanks,
Paul
Hello: Thank You for Your inquiry. These tweezers are plugged into a solder station. They do not plug into the wall.
https://www.sra-shops.com/pub/media/docs/srasolder/datasheet/tds-aot-macro-tweezers.pdf
The AON-1305 are a related product for AOT004, meaning these tips will fit these tweezers.
There are 110vac and 220vac version availalbe
T4206429
Check out Digi-Key’s TechForum for assistance anytime!
Were you satisfied with our service? Please take our short survey to help us improve.
Dave Bourque
Electronics Technician
Digi-Key Electronics
701 Brooks Ave S
Thief River Falls, MN 56701 USA
+1 800 344 4539 x 11371
Thanks. Are there other flat tips available?