Generic Solder Station Tip Needed

Hello,

I was given one of these solder stations that were made en-masse and sold for cheap, but AFAIK, no extra tips are available. It uses a hollow tip and can provide dimensions.

Maybe someone already has discovered a tip (like a Weller) that fits these?

It’s a pretty amazing unit that has survived a decade plus of use and abuse.

Cheers!

Hello,

I was unable to find a tip for this one.

Here is a link to the Weller tips we have in stock.

I think you’ll find these were rebranded by a few companies, one of them being
X-Tronic 4000 Series

I’ve heard reviews that people were using Hakko tips with the iron, but the thermal mass was heavier so it took longer to heat up. I’m also wondering if some Aoyue tips might work with those irons. Take a look at these tips to see if any of them look right

Here’s an example of the Hakko T18 series tips:

1 Like

Hi Kristof,

I looked up the tips w/dimensions and it appears what my station has is a T18BL. Will put one on my next order and will report back in a couple of weeks what I find, yay or nay.

Thank you all for your responses!

2 Likes

Thank you, it will be interesting to know what you find out.

For others reading along it also looks like these were rebranded as Gordak 952 Rework Stations

Update:
YES! The T18 tips work fantastic with this station. Probably will with all rebrands. :grinning_face:
The tip barrel is 2 or 2.5mm longer, so do NOT over tighten and crack the heating element like I did :tired_face: Still works though, LOL! Got lucky.

Cheers!

1 Like

Awesome, glad it worked. Thanks for sharing your information.