Hello,
I have a BBB (BeagleBone Black) and I wanted to find some headers for it. I checked online at mlelectronics and other sites. Anyway, I figured I could purchase them here from digikey.com.
These are dual row 23 position 2.54mm x 2.54mm connectors...
I am looking for the actual headers or something very similar. If you are aware of how I can attain these types of headers, please reply.
Seth
P.S. I searched online but only came across the through-hole tech. headers.
Hello @silver2row,
I reviewed the documentation for the Beaglebone Black, as well as our stock.
I believe I was able to find a similar option in PN: S7126-ND
As a related note, I do believe the original headers for the BeagleBone are through hole, but if you would prefer a surface-mounted option, I recommend you take a look at PN: 612-SSM-123-L-DV-A-ND
1 Like
Hello,
Thank you, sir. I just purchased them to find if the required parts will fit the BBB. The docs. do state they are through hole. I will think of the surface mount later if I have any trouble w/ the S7126-ND part(s).
Seth
P.S. I will update here once I receive the items and let you and others know if these parts work well w/ the BBB style headers.
We also carry the following, which comes as a set and is specified to fit the BeagleBone boards. They have long pins for stacking boards:
1528-1365-ND

1 Like
Hello @Jonathan_1325 and @David_1528 ,
Seth here. Thank you both for the reply. I ended up purchasing the S7126-ND solution for my project.
They came in yesterday and they work. Thank you both.
Seth