Does DigiKey carry BeagleBone Black with JTAG ?
@Stone2019, every BeagleBone Black has a 20 pin CTI header on the back you can use, from the manual:
5.12 CTI JTAG Header
A place for an optional 20 pin CTI JTAG header is provided on the board to facilitate the SW development and debugging of the board by using various JTAG emulators. This header is not supplied standard on the board. To use this, a connector will need to besoldered onto the board.
If you need the JTAG connector you can solder it on yourself. No other components are needed. The connector is made by Samtec and the part number is FTR-110-03-G-D-06.
Regards,
Thanks and do you also carry JTAG emulator ?
@Stone2019, sure, here is one of the TI JTAG probes:
https://www.digikey.com/products/en?keywords=TMDSEMU110-U
Regards,
Will this one work with TI code composer and BeagleBone black ?
TI CCS v7.0 and later: http://www.ti.com/lit/ug/sprui94/sprui94.pdf
Regards,