I have to replace a bleed capacitor 40uf one of two ,the nearest one the site is a Kemet C870CF35400AA0J and seems to be the same spec .The resistor on the original is difficult to identify it is ivory in colour with yellow,violet,yellow and gold band at the end.I believe its 470,000. It is 10mm long x 3.7mm diameter with 0.6 leads. What part /wattage should it be for the best 0.5 or 1.0 watts?. Its for a single phase machine with three 2.4kw motors
I also get 470k Ohms when I punch your colors into DigiKey’s handy Resistor Color Code Calculator
Here’s a 470k 5% 1W in roughly the dimensions you measured.
2 Likes