Can an actuator be incorporated later?

Question:

Can an actuator be incorporated later?

Block

Answer:

Omron’s V size basic switches have optional actuators (VAL, VAV, VAM) that can be incorporated later.

Block

Explanation:

The following actuators can be incorporated later:

  1. Type VAL: Leaf spring type
    Suitable to operate a basic switch with relatively less frequent rotary cams or sliding.

  2. Type VAV: Hinge lever type
    Can be used where a small operating force (OF) is required.

  3. Type VAM: Reverse hinge lever type
    Operation is reversed and excellent in vibration and impact resistance. Since the overtravel (OT) is large, it can be used for automatic control of machine tools and door switches.

  4. Type V-VAQ, TypeSS-A2A
    Basic switches can be used in the same way as push buttons.

Block

Quick tips

In some cases, the standard type lever cannot be set (the operating position cannot be adjusted). An actuator lever that will be mounted later can be processed before mounting. Please do not process the lever type; otherwise, a problem may occur.


Product category

Switches Basic Switches


Classification

Selection, Characteristics


Related keywords

Basic Switch
Lever
Actuator
VAL
VAV
VAM

Block

Please visit the link below to see this product category on the Digi-Key website
Switches | DigiKey Electronics


This FAQ has been brought to you courtesy of




Please click the link below to view the original FAQ

https://components.omron.com/us-en/faq/switches/FAQE20011