Hello!
I have researched this a bit but need to ask the professionals.
This belongs to a Tajima Embroidery machine from the mid 2000s. Japan built.
Can anyone help me identify the connector and the pins that go with it?
The Connector reads JSTH
The pin reads 5JST0
I’m about to stick some rectangular header pins into that socket, but i would love to have a complete repair.
Thanks for any input!
Hello @matt.girouard
Take a look at the PHR-3 There are some similar products from JST if the pitch is not right.
Contacts can be found in the associated products depending on wire size and plating.
-Robert
Incredible thanks so much
Will these crimped terminals work in this connector? They were in associated products but the cart was being glitchy with the bare terminals.
Hello matt.girouard,
Yes, it does appear that those would work together. We also have all of the pre-crimped leads linked HERE should work with that PHR-3 connector.
incredible service. Thanks so much
Its a little overwhelming but I got the hang of it haha.
The wires that are currently on there are 26AWG.
Would this still be ok to repair this harness?