Frustrated looking for JST PH2.0 Tins

After looking around trying to figure out how I find pairs of JST tins that work together. I wish the site had a better way of showcasing ‘hey this is the corresponding set of connectors that are used with this’ so I could cross check to make sure what I was buying was going to work together. There are a plethora of models, series names, and variables in the naming scheme of each connector. Maybe I am too noob to understand that SPH, and SPNI are so different when I am looking for the male pin and female version of the same thing both being P0.5. I am trying to find the tins used in the JST PH2.0 plug. The same you find on the amazon crimp kits. Problem is the DigiKey search is useless for this task, especially while Aliexpress gets it immediately. I want to buy through DigiKey because I like the service and I feel better that it would be made with better quality material or whatever. Aliexpress has inconsistent shipping etc. But I do not know how to find it, and I cant really confirm whether it is even listed, it could not exist I would have no idea because searching for things is very complex. If someone could point me to the male pin version for wire to wire connections it would be appreciated. I did manage to get the female version (455-1127-100-ND)

Thanks!

Oh and I am also buying these to work with existing connectors that I already have. But I dont know what the technical part number is as they are an Amazon source (said kit). It doesn’t really help looking around for JST PH2.0 as there are variants of the connector type or something I don’t yet understand.

@erosion139

I understand that trying to find the specific connector that is similar to the ones from a kit from from Amazon can be tricky as in most cases they would not reference the manufacturer item numbering at all or even the series name correctly either.

For the PH2.0 you reference I would think that would be the PH series we list that are 2.00mm.
An example item would be PHR-2
For that item we do list near the bottom the Associated Products for it, which include the contacts that can be used as well as options where we have already crimped some wire on if needed.

We also do list he manufacturer recommended mates for that too.

As for the general quest to find the specific JST connector that can be a bit tricky too, as JST does indeed have a fair few very similar items.
If you have the images of the item you are looking to replace and mate to we can take a look to see if we can assist in matching up to what you have on hand.

Sorry for the late reply. I took some of the best photos I could of the connector. Hopefully you or someone else can recognize it easier than me. I would imagine its common maybe, but I am not sure. Not many cases where I see a wire to wire JST setup versus PCB mounted sockets.

@erosion139

The most similar item I had found for the contact in the image are the below.
I am sorry to say that I did not see a JST item that looked like the imaged contact.
123-A-WBT-D002EG-01CR02TR-ND
A-WBT-D002EG-01CR02 Assmann WSW Components | Connectors, Interconnects | DigiKey

WM15203CT-ND
1510878101 Molex | Connectors, Interconnects | DigiKey

If it is of any help we have pre-made 200mm male pin cables that are compatible with two position JST PHR-2

Adafruit Part Number 3814

The issue is that JST doesn’t actually make very many connectors with male crimp pin versions, and many of those don’t have wire-to-board versions. Two of the most popular JST series, XH and PH, are among the many that are strictly wire-to-board, and thus only have female crimp contacts. (It also doesn’t help that JST sometimes has compatible connectors, but gives them a different name. For example, the female board-to-board version of XH is called JQ.)

Chinese clone vendors sometimes make these “missing” parts, and male PH and XH crimp are an example of this. So for these, only clones are available.

FYI, if you want genuine JST series that have both wire-to-board and wire-to-wire versions, look at the PA/PAL (2mm) and XA (2.5mm) series.