You can put as many surge suppression ICs in parallel as you want. The I-trip would add up. So two 500 mA Itrip should be around 1 A I-trip. Note, however, Bourns doesn’t recommend putting TBU® in series. You can gain current capacity, but voltage rating is what is stated on the datasheet.
ProductExample
| MFR PART # | P40-G240-WH |
|---|---|
| DIGI-KEY PART # | P40-G240-WHTR-ND |
| MANUFACTURER | Bourns Inc. |
| DESCRIPTION | SURGE SUPP TBU 240MA 40VIMP SMD |
| DATASHEET | Click Here |
Please visit the link below to see this product line on the Digi-Key website
Circuit Protection | Surge Suppression Ics | Digi-Key Electronics
This FAQ has been brought to you courtesy of
Additional resources that may prove useful.