Capacitor Identification for Lennox 10F81 Thermostat

I am trying to determine replacements for 3 capacitors on for my Lennox 10F81 thermostat. See attached pictures. Appreciate any help you can provide. Thanks!

Hello mcerone14,

What are the dimensions of the caps (diameter X length), and also the dimensions of the base, for the first two? Click here for options for the first one.
The closest match to the second one, is PCE4798CT-ND, please verify the dimensions.
For the last one, they appear to be through hole leads. Click here for some options.
You should check all the datasheets to verify compatibility.

Hi David_1768,

Thanks for the quick response.

Here are the closest measurements I can get for the dimensions you requested:

47UF 10V: 5mm diameter x 6mm length. Base appears to also be 5mm
220UF 50V: 10mm diameter x 11mm length. Base appears to also be 10mm
1.5F 5.5V: 18mm diameter x 5mm length

Yes, the last one does have through holes.

Thanks