Capacitor type

------Question for B43501A3337M000 Please Put your question below------

The item we require is: B43501A3337M42 330 uf 385v

What is the difference between M42 & M000 ?

Also, our items are 3 pin solder type mount, can DigiKey supply these ?

Thanks

Hello,
Welcome to the DigiKey TechForum. I wasn’t able to find what the 4 is in the suffix but 2 is the callout for 3 terminals which is DigiKey part 495-75216-ND. This is a nonstock item so you may want to look at DigiKey part 495-B43501A9337M002-ND as a possible alternate and currently in stock. Note that the height of this capacitor is taller at 47mm.

Thanks Steve

Just a couple of things re: 495-B43501A9337M002-ND

Will the voltage difference cause any issue 400v vs 385v ?

And our current units are 3 pin solder type not snap in.

Sorry if the questions are a bit simple but we are more mechanically focused.

Hello,

The capacitor having a higher voltage rating will be ok as this is just a maximum rating for the part, and the snap in style means that is has bent leads that help hold it in place when soldering to the board.

Many thanks Rob.

Are the 495-B43501A9337M002-ND available UK supply ?

Thanks, Wal

I believe these can ship to the UK, but I would advise checking with our sales team to confirm.

If it is listed on the UK version of our website, then they should be able to be shipped there.

Looks like it is:

495-B43501A9337M002-ND