I’m wanting to buy these connectors and leads:
But I need to find a panel-mounted part to connect it to, along the lines of
Failing that, I need something similar with a right0angled connector that is not a 2.1mm connector. I have 24V and 12V with identical 2.1mm central pin connectors. I want to change the 24V one to something else to prevent user error. Max of 245V 0.5A DC
Needs to be right angled connector on the lead because of where the socket will be installed.