Co2 infared sensor

Hello anyone , im have three sensor CapOne from nihon kohden , three sensor have the same fault , after connecting the device does not feel the sensor, i checked the capacitors ont the board but i cannot identify the elements with the 4CT marking code, it has x29 engraved on the bottom. Any help is very helpful


Thank you for your inquiry.

I’m striking out on finding a part associated with those part markings.

Hopefully someone else might have something to add…

Hi oppomlody,
I don’t understand what kind of sensor this is.
Is it a CO2 or an infrared sensor?
Can you take a large photo of the top and bottom of the sensor?
Every letter, dots and line of the marking has a meaning.
Also need chip dimensions.

hi its sensor co2 . for human parameter monitor. yes im attached

1 Like

oppomlody,
Please unsolder this chip 4CT.
Wash it thoroughly with alcohol.
Take a good quality photo from above and below.
Take a photo of the marking from different angles.
Please provide the dimensions of the chip.
Each letter, number, dot, and dash on the marking is very important.
I found the name of all the chips on the board, except for 4CT.
D6Q - EMZT6.8E
J0A - AD623ARMZ-REEL7
A12X - IP2112A
A48, (S48) - OPA348AIDBVR-MS/OPA348AIDCKR-MS
T7U - TL431AQDCKR
14_CZ - SN74LVC3G14DCUR

1 Like

yes data its correct , im found 70% of these , for ip2112a not have 100% sure. thank you

Check this link:

Can you check dimensions of the chip?
Are these dimensions suitable for the chip 4CT 821 ?

1 Like

look these XC6351A120MR Charge Pump PMIC SOT-163/SOT23-6 marking A12 Charge Pump Voltage Inverter IC|Welcome to Eric Online Store - Shenzhen ERIC Electronics Co., Ltd. , today measure element

This is not XC6351A120MR.
It has the following marking rule:

2 Likes

This is a quick hand drawing.
There may be mistakes.
Can you draw something similar?

3 Likes

thank you for u time and work , attached photo.



pin 1 Gnd emmiter , pin 2 power 5v emitter ( ir ) , 4-5 Gnd , 6 - 8 collector

Yes the same

Any help how its it 431?

Please, draw something similar.
I can’t help you without your participation.

Where do these wires go?

Adam7,

The first picture, at the top of the post, shows the other side of the board, with the wires and traces.

Hi David_1768,
Maybe I’m not explaining it correctly.
I’m wondering where these wires go.
In the photo I see that the wires go to some device.
I’d like to know what it is and see the whole device.
But the creator of the topic is silent for now.