Confirmation on capacitor's value

Good day! Could someone please confirm a capacitor’s value. I’m not sure whether this value is correct. The information printed on the polypropylene snubber capacitor itself is F.0145H. Is this a 0.0145uF or a 0.145uF?

Hi @norloonda2
Can you please share the capacitor’s part number?

A picture showing the part’s marking would be helpful on this.

Thank you for responding. I don’t have a device that can that a picture of that exact capacitor but, I will send a picture of the of the exact configuration of capacitor in question. See attached picture. This is as it’s printed on the body of the component itself F.0145H / 1600v. It is a component on a 1989 RCA Colortrak 2000 Stereo monitor console.

The stock number as printed in the Master Service Manual is 195700. This may be a vender’s reference number.

I do not have photographing capabilities. I can only show the exact configuration / image of the polypropylene capacitor that has this information on it.
F.0145H 1600V. The Master Service Manual parts list and capacitor image attached.

Sincere thanks,
J. Wright

(attachments)

Supplemental information. This part is a component of an RCA Colortrak 2000 stereo monitor console.

0.015UF is the closest I can find.

ECW-H16153JV Panasonic Industry | Film Capacitors | DigiKey

Thank you Kristof. My computer is slowly pulling up the information that I can evaluate the mechanical footprint - This is critical. But the primary information I was seeking is a confirmation of the information on the value. From observing the attachments, the value of the capacitor is 0.0145uF (0.015uF), not 0.145uF (0.15uF)?

That is correct. 0.0145uF

Thank you. I;m working with “AI” and like the caution says, AI does make mistakes! I just needed an experienced human who knows.