Confirmed part needed

Hello, I think I have a good idea of what I’m needing, I just need to confirm because the relay is from an alternative manufacturer so I can’t be quite sure of the specs.

It’s a PCB relay, the model on it I SCH-T73-1C-24S.

Other info on the relay:
15A 125VAC
10A 30VDC
10A 277VAC

TGD26 PTGY 24VDC

The manufacturer was Xingchuangzhi

I think it’s a NO relay based on it being for a motor actuator. I found a Potter & Brumfield T73 relay, just want to make sure I get the right one.

Thanks!

thomas.borkowski

Thank you for contacting DigiKey , from what I am finding for the SCH-T73-1C-24S this is a 1 form C relay , which makes it a SPDT relay , the T73 series from Potter Brumfield is obsolete , I did find a part number that we have that looks like a good replacement it is our part number 3385-AZ943-1CH-24DE-ND , check data sheets to see if this will work for you and the footprint on your board .

Thanks Craig

Thank you so much Craig! Dimensions all match.