Hello!
I’m trying to find a replacement relay for the pic attached. There was no outer cover, so the only numbers I could find where the ones seen in the photo.
I know it is supposed to be a 24v.
This is for a vintage stereo receiver.
Thank you for any help!
Dennis
Hello Dennis,
The image for some reason did not attach. Can you try to resend it?
@dennisfrancis
Images can be added to the post by dragging the image into the field with your response or question(for future posts.

Or by using the up arrow icon shown above to search for it in your system.
Ok, I posted a new reply with pic. Might be under a different category? Sorry, the section is a little hard to navigate sometimes.
Hello Dennis Francis,
Some further detail would be helpful in locating possible alternatives. Such as the number of pins as this can be helpful in determining the contact form. Since this is a board mounted part the board layout for the pins may be helpful with matching up. I see you referenced this as a 24V relay I assume this is the coil turn on voltage. Sharing any details regarding the load side voltage/current as well.
Best regards,
8 pins total, 4 per ‘side’ pic attached of bottom PC board
We would still need a little more work on your end as we have so many to chose from.
- is it 24 VDC or AC?
- what is the spacing of the pins for example I have 2066-55.32.9.024.0040-ND which may match the pattern on the board hard to be sure with just a picture.
- we have two categories power relays over 2 amps and signal relays for less than 2 Amps.