Connector 3-pole DIN 9680 identification

Hello
I am looking for the 3-pole DIN 9680 female base connector 4 6.3 mm / 1 4.8 mm flat female connections with folding box and screw cap according to the attached photo. The original part number for the Hella brand is 8JB 001 933-042.
what will be your replacement?

Thank you very much

Best regards

Din 9680

Have you tried 82005494

hello maxicastiglioni,
It looks like that particular connector Hella brand 8JB 001 933-042 is used as a Power connector on Agricultural Equipment. this document explains the DIN 9680
I am sorry, but we do not have that exact style of connector and do not have a Direct mating or replacement for it.
If you are looking for that exact style I would recommend checking with a Farm Implement Dealer

Hil matt

the search with that code does not return results

Sorry, I didn’t mean to imply that it was a part number that was available on Digikey

Hi matt

searching I found the part 18-00681762-ND - Manufacturer Product Number 00681760 Supplier Littelfuse Inc.but it is not available. Will there be any from another manufacturer?

There appears to be many manufacturers. Just not available through Digikey. What is your goal? Are you trying to find a cheaper alternative to the manufacturer that you originally provided?

18-00681762-ND is the only 3 position DIN9680 I saw in our system.

image

DatasheetIMPAGINATO EPS 2007.indd (littelfuse.com)

I also found the DIN9680 parts on TE Connectivity: Connectors & Sensors for Harsh Environments. The parts start with the prefix CAR… Unfortunately, I don’t see any of those parts in our system at this time. TE is a supplier we carry. So, if any of those options would work, we might be able to do a Non-Catalog request to find the manufacturer’s minimums, price, and lead times. Note: the contacts might be sold separately. Check the product page on TE for the associated contacts that would also need to be quoted.

If you would like a quote on any of the TE parts, send the full mfg part numbers and all your contact info to applications.engineering@digikey.com. Turnaround time is 3-5 business days for the quote.
.

Hi Jeff
excellent contribution,
I am going to send an email to quote.
Thank you very much

Best regards