Unpacked, installed antenna’s hooked up the serial cable to my usb to serial adapter and followed the instructions on the setup wizard.
I started with client and the wizard found it, I set baud to 9600
Then the same with the server.
I plugged them both in approx 15 to 20 ft apart, placed a paperclip in pin 2 and 3 on the client for loopback test. verified both units had power light and Link light and tried to test for loopback and do not get a successful loop back test.
I tried connecting the device and cannot communicate with it either.
The device does communicate if plugged in directly to the USB to serial adapter.