I need to know the part# for the power cord that is used with PEAD65-12-B2
Hello glomeo and welcome to the DigiKey TechForum. The reason there are no cords for this is because there are a few cords that can work with it. You can find those options by clicking HERE.
There are actually quite a few cables that are potentially usable; however if one searches cables by the listed socket type (IEC320-C14) on the power supply one’s not likely to find them, because one wants a cable with a mating plug type, which would be an IEC320-C13. This link would perhaps be a better one for global use, while if looking for a cable suited for use in the US or other localities using similar plug types, this link would be one to choose from.