When it comes to LED’s, one important aspect is the Binning that they are in. The Binning can be explained as the group the LED is placed in according to its color. Digi-Key does not separate the LED’s into different bins. If a certain Bin is required, please email the binning information and requested quantity to orders@digikey.com.
In this example we will be using the part number Cree part number CXA2520-0000-000N00R250F-ND .
On the Data Sheet for this LED there will be a Order Code and a Bin Code part number breakdown.
The Bin Code will be found on the Manufacturers Label.
The Bin Code for this part will be CXA2520-50F-S2-N0B-000A4
The Order code is the part number CXA2520-0000-000N00R250F
Order Code Breakdown
Series = CXA25
Performance Class = 20
Internal Code = 000-000
Vf class = N0 = 36-V class
CRI Specification = 0 = Standard CRI
Kit Code = R250F

Bin Code Breakdown
Series = CXA25
Performance Class = 20
Chromaticity bin = 50F
Flux bin = S2
Vf class = N0 = 36-V class
CRI Specification = B - 70 CRI minimum
Kit Code = 000A4

The key Bin Code parameters are:
Flux Bin
S2

CRI
70
The chart that does show the parameters together is:
This will show that the part will fall into the 3A0,3B0,3C0,3D0 Regions.
For any definition examples please check out the LED Terms post.