Checking on the company website, I believe I need to order item CREE XP-E2 # A007-CG2H-765S4 (6500K) but am not completely sure.
Could you please advise me on the correct replacements to order for my application?
I have attached an image of the CREE LED (approx. 20mm diameter) and the power supply (info) feeding it.
Any help would be much appreciated!
Hello joneswpg and welcome to the DigiKey TechForum
The part number you provided leads me to 788-A007-CG2H765S4-ND. This does appear to use a Cree XLamp XP package though. From what i could see for specifications on the datasheet, it should work with 2.7V and 350mA. Your driver should be able to power this, as it has a constant current output of 350mA and voltage output of 0.5 to 10V.
I did also find the options linked HERE that should work with 350mA, a voltage within your outputs range, and are close to that 20mm diameter (around 19.90mm). These do have a different CCT(K) value, which would be used to determine how white your light would appear. The lower the value would be more yellow, and the higher value would be bluer.
Thanks Nick. I’ll check out your suggestions.