Cross-Reference for Genteq HVAC Fan Motors & Capacitors

Hello everyone,

I’m looking for assistance in finding a suitable replacement for two specific Genteq exhaust fan motors and their corresponding run capacitors. I need to source these for an HVAC system repair in Saudi Arabia.

Could you please help me identify a cross-reference or a 100% compatible alternative from DigiKey’s stock for the following components?

Motor 1:

  • Manufacturer: Genteq

  • Model: DE2F090N

  • Specifications: 1/6 HP, 1550 RPM, 115/220V, 50/60Hz, 2.0A, Single Phase

Motor 2:

  • Manufacturer: Genteq

  • Model: DE2G109N

  • Specifications: 1/7 HP, 650-1750 RPM, 115/220V, 50/60Hz, 2.0A, Single Phase

Capacitor (for both motors):

  • Rating: 10 MFD (Microfarad)

  • Voltage: 370VAC or higher

I have attached photos of the original motor nameplates for reference. The most critical factors are the electrical specifications and the physical dimensions (frame size, shaft diameter/length) for a direct replacement.

Any guidance on finding a suitable match in the DigiKey catalog would be greatly appreciated.

Thank you for your support.

Best regards,
Faisal

Welcome to the TechForum @faisal.ali ! It looks like the pictures did not attach in your post. The button is on the far right when you start making a post, see below:
upload

Regardless, we don’t seem to have suitable alternates in stock for the motors. The highest wattage we have in stock at 115-220VAC is 35W which is approximately 304mA. As for the capacitor, what kind of capacitor do you need? There are a lot of different styles. Most likely, you’d be looking for a motor starting capacitor, unless you mean something else.