Current Divider Guided Learning Q3 – What is the current divider equation?

This article is part of a guided learning series exploring the theoretical and practical aspects of resistors in parallel.

:pushpin: Canonical Article: Current Divider Formula and Derivation
:blue_book: Learning Companion (Q&A): Explore All Questions

You are reading: Question 3

What is the current divider equation?

Answer

The current divider equation allows us to calculate the current in an individual resistor when given:

  • a constant current source

  • two or more resistors in parallel

Introduction

The primary article presents several useful equations along with the associated derivation.

These equations are found across multiple textbooks with a strong dependence on the students’ knowledge and growing mathematic skills:

  • Elementary textbooks will focus on a two-resistor solution.
  • Advanced textbooks will generalize the equation for multiple resistors.

The best equation is therefore a journey toward the most generalized form. This reflects the engineering mindset to commit routine calculation to muscle memory. For instance, a 3rd year EE student has performed hundreds of parallel circuit calculations. The patterns are ingrained, and they hardly stop to consider if the circuit has 2 or 10 parallel components. Either way, the algorithm is the same.

The aspirational (recommended) equation

The equation is the best solution as it represents the current divider in its most abstract form.

I_{R_X} = I_{Total} \left( \frac{R_{Total}}{R_X} \right)

Where:

  • I_{R_X} is the current through the resistor of interest
  • I_{Total} is the total current
  • R_{Total} is the equivalent resistance of the parallel resistor combination
  • R_X is the resistor of interest

Tech Tip: There is an old truism implying that we learn the Fall semester material in the spring. That certainly applies to the 1st semester DC voltage divider. The true muscle memory is formed in the 2nd semester after performing hundreds of equations using AC circuit analysis. While DC and AC are related; we must now account for the complex impedance of inductors and capacitor.

Two parallel resistors equation

This is the common textbook presentation for two resistors.

I_{R_1} = I_{Total} \left( \frac{R_2}{R_1 + R_2} \right)
I_{R_2} = I_{Total} \left( \frac{R_1}{R_1 + R_2} \right)
Where:

  • I_{R_1} is the current through resistor R_1
  • I_{R_2} is the current through resistor R_2
  • I_{Total} is the total current
  • R_1 and R_2 are the resistances of the respective branches

As a teacher, the most common error I encountered was placing the wrong resistor in the numerator. This is easy to do as there is a crossing pattern such as when we calculate R1’s current with R2 in the numerator.

Error-prone equation

There is a third version that I strongly recommend you avoid for the reasons listed in the canonical article. For convenience, here is the amplifying text:

Occasionally we encounter a third variation that attempts to generalize the previously mentioned two parallel resistor equation. Personally, I do not like this equation as it requires a picture to explain. It also adds an unnecessary cognitive load, requiring us to differentiate between the “equivalent parallel circuit resistance” and the “equivalent parallel resistance of the circuit excluding the resistor of interest.

Tech Tip: Recommend you avoid the error-prone equation. I’ve seen too many students confuse the related but subtle distinction between “equivalent parallel circuit resistance” and “equivalent parallel resistance of the circuit excluding the resistor of interest.” We will not address this error prone formula again.

Related safety note regarding parallel resistors

When I was teaching my students would poke fun at me by saying, “current takes the path of least resistance.” Words can’t explain how much that statement bothers me, as it is fundamentally wrong and can even lead to safety hazards. For the record, current takes all paths, and you don’t want to be in any of those paths.

:writing_hand: Article by Aaron Dahlen, LCDR USCG (Ret.), Application Engineer at DigiKey. Author bio.