When looking for a AC to DC power supply, sometimes there isn’t a readily available solution with the required Voltage / Current output’s. In this case, we do have a configuration wizard on our site, that can provide all the parts needed to assemble the power supply.
This link Excelsys Configuration Tool (digikey.com) will bring you to the the configuration wizard as seen below.
Simply complete the table with your requirements, and it will do the rest!
The Excelsys Configuration wizard will configure a power supply to meet your exact power requirements, which will load the proper AC DC Configurable Power Supply Modules along with the proper AC DC Configurable Power Supply Chassis from Excelsys / Advanced Energy only. If no results render, then another configuration will have to be applied that fits within their offerings.
For an example, I will use 10V @ 20Amps, 12V @ 30Amps, 6V @ 15Amps, and 7V @ 12Amps.
After the values are entered, click on “Configure Unit” and all the Manufacturers Part Number’s, quantity, instructions, and price will be listed as in the example below.