Can you suggest me a DC-Dc converter which converts input voltage 37.5VDC to 12VDC and current range upto 5A and it should be mounted on DIN rail and it should satisfy MIL standard or below compliance certificate required.
IEC 60571- 2012(Railway application)
EN 50121-3-2(Electromagnetic compatibility)
IEC 61373 (Shock & Vibration)
sreekanth.aare
Thank you for contacting Digi-Key , sorry we do not have a DC to DC converter to offer with those specs .
Thanks Craig
Hi sreekanth.aare,
It looks like the DDR-120C-12 meets your requirements.
From page 3 of datasheet:
If you could manage with a panel mount variety, the following might also be worth consideration:
That one did not show up for me Good catch David
Thanks David. It suits for my requirement. My procure team will place the order.