DC motor Hall sensor/ switch

Having problem getting the correct hall sensor/ switch for DC hub motor on a scooter.
I ordered some last week but the output voltage was not high enough.
It was only 2.5V
The control voltage is 5 volts. And I need an output voltage of 5volts.
The number on the original sensor is S41327. This sensor is no longer available.

Hello Kcona3, thank you for contacting DigiKey Technical Support.
These are all the 5volt options we carry.
The output is rated in amps not voltage.

Any idea which one would copy the characteristics of the the one I have.
This is the number on the original hall sensor.
Part #S41327

The supply voltage is 5v
And the return voltage needs to be as close to that as possible.
The ones I purchased last week only put out 2.5v and the controller does not see it. The voltage is too low.

If you are looking for a replacement, you can check Honeywell SS41.