Difference between S34ML08G201BHI000 and S34ML08G101BHI000

Hello ps1,

Looking at the datasheets, the difference appears to be the NAND technology used in the IC. For the S34M08G101BHI000 it uses Spansion Revision 1, which is a NAND flash memory with a 4x nm process. The S34ML08G201BHI000 uses SkyHigh’s Revision 2, which is a type of NAND flash memory with 32 nm technology.
Comparing the two, it looks like the S34ML08G201BHI000 has a newer generation NAND technology that provides higher memory density and better power efficiency compared to the S34ML08G101BHI000.