Hey everyone!
I’m working on creating a mock disc brake setup to demonstrate braking, and I’m trying to determine what type of electric motor I would need (with a variable speed control) to attach a rotor to that would give me around 3000/3500 rpm?
Let me know if you need any further information.
Thanks,
Josh
Greetings,
A plain 'ol brushed DC motor fed by a variable-output bench supply would probably be the most straightforward approach. The “CIM” motors used in the FIRST robotics competition aren’t ridiculously priced and are large enough to make a reasonably visible demo. Downside is that a relatively large bench supply like the 382275 would be called for if a person wanted to give it a decent workout. A likely cheaper if less convenient option may be to get an appropriate motor controller from the same source you get the CIM, and feed it from a 12V battery as is the fashion for the FIRST competitions.
Hi @swdeveloper
A scooter motor and speed controller may also be an option coupled with an AC/DC Converter of proper voltage and wattage, I believe most are 36v but can vary. Ebay should have either a kit or sold in separate pieces. For smaller applications you could use a radio control brushed or brushless motor and ESC with a proper ac/dc converter.
You can use a scooter motor, a speed controller, and an AC/DC converter. You can also use a brushed of brushless motor, an ESC, and an AC/DC converter.