Flex ATX PSU Recommendations with PCIe connector support for dedicated GPU

Hi, I would like to have some recommendations for Flex ATX power supplies that match the following requirements:

  1. Flex ATX, 5.90" L x 3.21" W x 1.59" H (150.0mm x 81.5mm x 40.5mm)
  2. Around 500W
  3. Must have 6+2 pin PCIe connector for dedicated GPU usage.

I tried my best to search for power supplies with these requirements, but there is no listing that fulfill all of the requirements. However, I have found one power supply unit that matched exactly the requirement, FSP650-50FUB, outside of DigiKey website, which does not exists within the DigiKey website.

Is it possible to have a quotation on this product for me to make an order in Malaysia, or suggest me some alternatives that match the exact requirements?

Thank you and have a nice day.

If your dimensions are not limited to exactly the dimensions you provide, there is the Digikey PN 2967-FSP500-50FDB-ND (FSP PN FSP500-50FDB. Dimensions are 150 x 81.5 x 40.5 (mm) I used a EPS12V to PCIe 6+2 adapter to power an Nviidia 4060. using this PSU. It can be found on the FSP website under the industrial subgroup of power supplies.

nominal 500W 624W peak.