I am working on a Water Flow Test Stand at the University of Southern California. We are considering the ifm SU8621 flow sensor for installation in a nominal 1-inch water line and would appreciate your guidance on calibration and suitability for our application.
Our system uses compressed air to pressurize a water tank, driving water through a control valve, past a pressure measurement point, and through a test article. Only water flows through the sensor. We use volumetric flow rate and the pressure drop across the test article to calculate its flow coefficient, Cv.
Currently, we calculate flow from the change in collected water mass measured by load cells. We would like to introduce real-time flow measurement and improve accuracy. Because we have concerns about the accuracy of our existing load cell measurements, we are looking for a way to calibrate and validate the SU8621 against an independent reference.
What calibration method would you recommend for this application? Would timed water collection using a separate calibrated scale be suitable, or would you recommend a calibrated reference flowmeter? We would also appreciate guidance on how to apply any calibration correction to the SU8621 and what accuracy we could reasonably expect after calibration.
Could you also clarify the installation requirements, including straight pipe lengths and placement relative to the control valve, and whether you offer calibration services or recommend a calibration provider?
We would be happy to provide a plumbing diagram and additional operating details if helpful. Thank you for your time and guidance.