Hi,
I would love some help with finding the right capacitors for the ASUS Z790 Hero which I have here. The board came without capacitors around the CPU, so I can’t tell from old parts what I need. I identified two capacitors on the board, close to the CPU area:
FP10K 39Cz 561 6.3
FP10K 3YCz 271 16
One between the PCI-e slots:
FP10k 3YCt 101 16 (I believe it’s a ‘t’, not entirely sure)
I also directly emailed ASUS regarding the missing capacitors, but knowing their support I may not get an answer. Is there any way to figure out which capacitors are missing?
Cheers,
Al