looking to find out which connector and pins I have… I have put a new 2.3mm next to my existing pin for comparison…my existing pin is 3.5 +/- mm…
the pins are broken, so my best measurement is 6mm… but if you can point out the most similar ones with the same opening, and the compatible pins, I don’t have an issue ordering a few of them to see see which one ends up fitting… the opening (female side) is 7mm tall x 13mm wide…
What is the center-to-center pin spacing?
i believe 6 or 6.1mm
look correct now that I cross referenced with inches ![]()
there are many contacts, what are the differences?
I am using this in a marine application
Some of it will be wire gauge. You can also click on the data sheets of what you are interested in. This will break the parts down farther for you.