Hello, I’m wondering if somebody can identify the part number for the fuse holder attached. I’m looking for the cap part that holds the 6x30 fuse. Attached our photos of the front and of the holding mechanism. These were used in the Niles audio amplifier and the part broke. Thanks
Hello,
I was able to find 283-BK/HVP-LW-HH-R-ND, which is the closest to 6mm x 30mm I was able to find. Unfortunately, I did not see anything similar that specifically states 6mm x 30mm.
The reference to a 6x30 fuse may cause some confusion; I suspect that it’s meant as a reference to the 0.25x1.25" nominal fuse size commonly found in UL-rated often found in equipment of North American origin.
One solution in that case may be to replace the entire fuse holder mechanism. Another less-reliable option would be to check the Circuit Protection Accessories family for replacement end caps to a fuse holder assembly. I say “less reliable” because without identifying the holder assembly, it’s hard to be confident that any replacement cap that looks close would actually fit.