Hi, can someone help me identify these components?

Hi,

Can someone please help me identify this capacitor please?

Also, can someone please help me identify these 3 components: ?

Thank you,
James Pedersen

Hi @james00090 what is the mac model on the motherboard? These will help in your search as there is a group of users documenting every component on these devices, based on Apples model number: Category:Apple Laptops - Repair Wiki

Regards,

33uF - 16V

@RobertCNelson This is a MacBook Pro 13-inch, Mid 2010.

Thanks @Adam7, you rock!

You are Welcome! :handshake:

image

Any idea on the part marking of those two chips? Seems like where they’re located they might be TVS/voltage protection.

@Kristof_2649

Here is a slightly sharper image of those two components:

James Pedersen

Thanks for the photos but still hard to decipher, what do you see stamped on the parts ?

If the diode is marked JS, then it is probably CH501H-40PT.

Here’s another photo of the two chips:

Here is a even sharper image of the two chips, using two magnifying glasses and the maximum magnification on my iPhone’s front camera:

The only part that I was able to find with a part marking of y0p is SSM2315CBZ-REEL7 I hope that helps