The transistor’s switching speed is dominated by saturation. This post and associated video demonstrate a Baker clamp to reduce the turn-off time of a 2N3904 transistor from 0.4 µs → 0.05 µs. The Baker clamp is a classic transistor circuit that allows us to immediately see the charge-storage mechanism operating in a saturated transistor. The Schottky diode makes it easy to implement.
Beginners mistakenly assume a transistor’s digital switching speed is defined by the current-gain bandwidth product. For example, the lowly 2N3904 has a f_T of 300 MHz (0.003 µs period). A simple circuit will be two orders of magnitude slower. The Baker clamp provides about an order of magnitude improvement but nowhere near f_T. This is a reminder that f_T is a small-signal characteristic for a transistor operating in its linear range. It should not be confused with the charge-storage dynamics of a transistor operating in or near saturation. Recall that “small-signal” describes operation near the transistor’s quiescent point.
The term quiescent point is meaningless in a digital switching circuit.
Key Takeaways
- A functional Baker clamp can be constructed using a BAT46 Schottky diode and a 2N3904 transistor.
- Positive: The Baker clamp will significantly reduce turn-off time.
- Tradeoff: The transistor is in a quasi-saturation state. Instead of a V_CE near zero, the transistor’s V_CE is approximately 0.3 VDC (one Schottky forward drop).
Last update: 07 Jun 2026
Baker Clamp Theory of Operation
The schematic of the Baker clamp is shown in Figure 1. The defining feature is a BAT46 Schottky diode connected between the transistor’s base and collector. To understand the operation, consider the transistor’s base node. We have two competing factors:
- The textbook V_BE is approximately 0.6 VDC.
- The BAT46 diode will conduct when the transistor’s collector voltage falls low enough to forward-bias the clamp. Specifically, when V_CE drops below V_BE minus one Schottky diode drop.
Taken together, we see that the transistor cannot fully turn on as the BAT46 diode steals the base current that would otherwise fully saturate the transistor. The resulting output voltage is approximately set by the Schottky diode’s forward voltage drop. Technically, the load will see V_S - V_CE.
Note that the Schottky diode has a distinct advantage over a conventional diode such as the 1N4148 because its forward voltage drop is lower, resulting in a reduced V_CE for the drive transistor.
Figure 1: Schematic of the Baker clamp using a 2N3904 transistor and a BAT46 diode.
The Baker Clamp is a Feedback Circuit
The Baker clamp is best described as a feedback circuit. The transistor’s collector voltage is fed back to the base via the BAT46 diode. It is also a non-linear feedback circuit as the clamp mechanism only operates when the diode is forward biased. This only occurs when V_CE approaches the sub 1 VDC clamp voltage.
Like all feedback mechanisms, this circuit is susceptible to oscillation. However, no ringing was observed in the breadboard setup as shown in Video 1.
Video 1: Author APDahlen demonstrates the Baker clamp. The video includes a breadboard 2N3904 transistor circuit with a live oscilloscope to capture the results. The oscilloscope shows a 2N3904 transistor turn-off delay of about 0.4 µs, which is reduced to 0.05 µs with the addition of a Baker clamp.
The Baker Clamp Provides Quasi-Saturation
Without delving too deeply into semiconductor theory, we know that a saturated transistor accumulates charge in the base region. Before it can turn off, that charge must be swept away. It takes time to clear this charge, resulting in the 0.4 µs delay shown in the opening section of Video 1.
The Baker clamp prevents the transistor from entering deep saturation. Without deep saturation, there is less charge to accumulate in the base. Consequently, the transistor can turn off faster.
Parting Thoughts
The Baker clamp is a critical waypoint on your path to understanding the transistor. Can we truly understand the concept without sitting on the edge in a quasi state?
About This Author
Aaron Dahlen, LCDR USCG (Ret.), is a Senior Applications Engineer at DigiKey in Thief River Falls. His background in electronics and industrial automation was shaped by a 27-year military career as both technician and engineer, followed by over a decade of teaching.
Dahlen holds an MSEE from Minnesota State University, Mankato. He has taught in an ABET-accredited electrical engineering program, served as coordinator of an electronic engineering technology program, and instructed military technicians in component-level repair.
Today, he has returned to his home in northern Minnesota, completing a decades-long journey that began with a search for capacitors. Read his story here.