Hello Scheme it forum,
Have viewed the tutorials but have some questions.
Working on a circuit that uses a PIR to turn LEDs.
Does not seem to be a schematic symbol for
a PIR, HC-SR501.
So went to Build a symbol. When that is click on
a new screen appears titled ‘Symbol Editor’
but there are no controls available.
So I tried Symbol Editor v2.0. The link
seems to be broken. It does nothing.
(The Open Design Starters does work.)
So a new project was started and at Custom Symbols in nav bar
on left: Custom Symbols > Symbol Primtives
I drug a Part Body Rectangle on to Workspace
Three pins were put on the rectangle, V+, Grnd and Signal out.
This a fairly decent represemtation of a PIR.
In Part Properties on the right naming the
Symbol was attempted. In the text box
labeled RefDes the text ‘PIR1’ was input
nut when the textbox is left it goes back
to the default value ‘U?’
Would like to change the pin designations to
V+, Grnd and Signal out from Pin1, Pin2 and
Pin 3 but while the Font Properties allows
the text display to be changed the Object
Properties does not make a change to the
‘Pin1’ text available.
Thanks.
Allen Pitts
Dallas, Texas