How to Select the Right Knob for Your Switch or Pot

A common question we get is requests for assistance with determining the correct knob to affix to a rotary switch, rheostat, encoder, or other shafted rotary device. This can seem daunting, but there’s help to be had.

First of all, we have our Product Selection Guide for Knobs here on the TechForum. This defines what all the filters in the Knobs section of our website mean, which is a great place to start. When seeking to translate all those filters into a proper knob choice however, there’s a few things to keep in mind.
Let’s use CKN11861-ND as an example to work with - how would we go about finding a knob for this product?

The most important specification for ensuring compatibility between knob and switch is Actuator Type in Rotary Switches, which corresponds to Shaft Size in Knobs. Any device with a rotary shaft should have a description in its filters of the style and diameter of that shaft. For CKN11861-ND, this is listed as a Flatted shaft, 4.75mm diameter. This means you would start by selecting 4.75mm as your value in the Shaft Size filter for knobs, like so.

image

This ensures the knob is correctly sized for your device’s actuator. But what about the “Flatted” part mentioned by CKN11861-ND? Sadly, this is not something you can search for in our filter system at this time, but in this case “Flatted” is a very common industry standard for any actuator shaft designed to be used with a knob. You can generally presume that most standard knobs will work with flatted shafts. Other actuator types such as knurled are generally meant for finger operation, while round shafts are less expensive or work with specific types of machinery.

You may also need to open up your search a bit depending on your specific switch. Our example switch, CKN11861-ND, has a 4.75mm shaft, but only one knob in our system matches this diameter precisely. To generate more results, we can also select “close enough” values that shouldn’t dramatically impede our system, such as 4.8mm (essentially identical) or 5.08mm, like so:

image

This still leaves us only three options for this particular switch, but that’s better than one.

The second thing to keep in mind for proper knob selection is Height in Knobs, which roughly corresponds to Actuator Length in Rotary Switches. This one is a little harder, and for best fit in a precision application you’ll want to check the datasheet for any knobs you’re considering, as our system does not list the depth of the shaft well in a knob but rather gives its overall height. As a general rule, you can assume that any knob will have an average shaft depth available of three-quarters of its overall height. 36-8554-ND, for example, has a listed total height of 16.8mm, but its datasheet lists a shaft depth (the ‘B’ dimension, in this case) of 14.5mm. This is significantly more than three quarters of the knob’s total height, but as a rough estimate 75% of total height will ensure you have plenty of overhead for manufacturers who may not be quite as generous as Keystone.

You should also factor in the actual actuator length you have to work with when selecting a knob. CKN11861-ND, our example switch, lists a shaft length of 14.86mm; this is from the tip of the shaft to the base of the mounting bushing. This length is practical in a device like CKN11861-ND which is intended to be mounted straight to the panel, but switches like RTAP31S12W25FS-ND mount to the PCB instead and have a longer shaft. This is because these devices are meant to project their shafts off the board and through a hole in the panel, meaning much of the length of their actuator is behind the panel and thus unavailable to mount a knob to. If RTAP31S12W25FS-ND is mounted 15mm behind the panel, for example, then it effectively has only 10mm of available shaft to mount a knob to.

With these ideas in mind, we can select 1722-1174-ND from Davies Molding as the best fit in DigiKey’s system for CKN11861-ND. Or, if this knob doesn’t work in our application, we now know what to search for in alternative switches that might fit better with a knob we do like.

If you have any further questions, don’t hesitate to contact DigiKey Applications Engineering, and happy part hunting!

Thank you for this helpful post about knobs for standard encoders! Can you provide some guidance for dual concentric rotary encoders?

An example would be the PEC11D Series from Bourns.

Switches like this combine 2 rotary encoders into a single panel location, so two knobs are needed for the same switch. The inner knob is a typical encoder knob that slides over a shaft with a flat side. The outer knob, however, is designed to slide over the inner knob’s actuator and keys into notches on the outer knob’s actuator.

Can you please recommend a knob set that would work with this switch?

Hello,

I am looking into this for you. Will let you know when I have the information.

Hello @brad-tot,

This part appears to be close:

I’m unable to verify the diameter of the inner switch shaft. The flat appears correct, but not the diameter.

Best wishes,

APDahlen

P.S. Request @raelynn.roen verify or locate a better solution.

P.P.S. The KN5700B1/4 appear close. However, the inner shaft does not look compatible.

Thank you for the suggestions. Do either of those options accommodate the vertical travel needed for the integrated momentary push-button?

I don’t have the time or resources to make my own knobs, so it’s difficult to proceed on a switch without a complementary knob. These knob options are better than what my searches turned up – which was nothing! Still, though, it would be great if switches that have non-standard actuators could be sold as a set or with a direct link to compatible knobs.

I’m also chasing after a dual gang pot, like the P08x series from TT Electronics. Again, though, I’m struggling to turn up a match for knobs. Any suggestions here?

Sorry, @brad-tot,

I’m an hour deep and have yet to find a solution from any source.

A request was sent to TT, maybe they can help.

We sell enough of these products that we should have an answer.

Sincerely,

Aaron

P.S. Any ideas @rick_1976 @David_1528 @Matt_Mielke @PaulHutch @heke @Gromit

I have taken a look myself and didn’t find anything that has not already been suggested. Apologies, Brad. I know APDahlen and many of those he mentioned are very good at finding answers, hopefully we can locate an option for you.

You could try the aviation simulation industry. It appears as though this is somewhat common for them.

Here is a knob set that looks nice: Dual level knob

This one comes with the encoder, but it isn’t expensive: Dual knob

There are also files for 3D printers to print your own knobs if you have a 3D printer. Both links above are made for the push button type encoder.

I hope this is helpful.

Mike

Thank you, @Gromit

Aviation!

r/

APD

Thanks, that is helpful.

Hi @brad-tot ,
Some guitar knobs are concentric dual. Cannot find D-type/slotted shaft compatible, but with a luck could perhaps use a screw tightened one. For push button action, you could put some padding inside the topmost knob’s shaft tunnel.

Cheers, heke