Question: How can you know the specific timing of a time-delay fuse?
Answer: Check the T-I (Time-Current) curve in the specification sheet.
Example:
| DigiKey Part Number | F1710-ND |
|---|---|
| Manufacturer | Littelfuse Inc. |
| Manufacturer Product Number | 0216008.MXP |
| Detailed Description | 8 A 250 V AC DC Fuse Cartridge, Ceramic Requires Holder 5mm x 20mm |
| Datasheet | Datasheet |
We can find the T-I (Time-Current) curve of this product in the Datasheet
As can be seen from the graph:
- When the current is relatively small (towards the left side of the horizontal axis), it takes a relatively long time for the fuse to blow, which may reach several hundred seconds or even thousands of seconds.
- As the current increases (moving to the right along the horizontal axis), the time required for the fuse to blow decreases rapidly. For example, when the current reaches a certain value, the blow-time may be shortened to a few milliseconds.
More Littelfuse circuit protection products
Littelfuse Circuit Protection products provide stable and reliable signal transmission guarantee for all kinds of precision electronic devices by virtue of their precise adjustment relationship with capacitance, dynamic resistance, etc. in terms of high-frequency characteristics, and their performance is excellent in the industry.
More Q&A on Littelfuse Circuit Protection Products Technology:
I. Questions Related to Component Characteristics
-
Littelfuse new MOV+Sidactor thyristor vehicle charging solution technological innovations
-
In Littelfuse circuit protection products, what kind of current is I in I²t?
-
What are the differences between discharge tubes and metal oxide varistors?
II. Questions Related to Selection
-
How to select metal oxide varistors for overvoltage protection?
-
Do Littelfuse overcurrent protection fuses/circuit breakers have self-resetting function?
-
The difference in the selection of overvoltage / overcurrent between AC and DC input terminals?
-
What parameters differ between surface mount and through hole fuse selections?
-
Under what general circumstances can AC components be directly used in DC circuits?
-
Can the method of paralleling small-capacity fuses be used to achieve the purpose of fast fusing?
III. Questions Related to Applications
-
What design requirements for overcurrent and overvoltage protection?
-
In which fields are gas discharge tubes mainly applied? Do they have directionality?
-
Are overcurrent and overvoltage protection for AC/DC power inputs used in charging piles?
-
Can Littelfuse Circuit Protection Products Protect Against Overvoltage and Overcurrent?
-
How to specifically know the time of time-delay fusing fuses?