Question: What fields are gas discharge tubes commonly used in, and do they have polarity or directionality?
Answer: There is no polarity. These devices are mainly applied in communication products (with low capacitance) and common-mode protection of power supplies.
-
Gas Discharge Tube Arresters (GDT) have no polarity. No matter how they are connected in the circuit, as long as the voltage reaches a certain level, they will work normally and discharge the excess voltage.
-
They are mainly used in communication products (due to their low capacitance, which can protect communication equipment from overvoltage damage without affecting the signal) and in the common-mode protection of power supplies (by diverting the excess voltage on the power line to the ground to protect the components of the power circuit).
More Littelfuse circuit protection products
Littelfuse Circuit Protection products provide stable and reliable signal transmission guarantee for all kinds of precision electronic devices by virtue of their precise adjustment relationship with capacitance, dynamic resistance, etc. in terms of high-frequency characteristics, and their performance is excellent in the industry.
More Q&A on Littelfuse Circuit Protection Products Technology:
I. Questions Related to Component Characteristics
-
Littelfuse new MOV+Sidactor thyristor vehicle charging solution technological innovations
-
In Littelfuse circuit protection products, what kind of current is I in I²t?
-
What are the differences between discharge tubes and metal oxide varistors?
II. Questions Related to Selection
-
How to select metal oxide varistors for overvoltage protection?
-
Do Littelfuse overcurrent protection fuses/circuit breakers have self-resetting function?
-
The difference in the selection of overvoltage / overcurrent between AC and DC input terminals?
-
What parameters differ between surface mount and through hole fuse selections?
-
Under what general circumstances can AC components be directly used in DC circuits?
-
Can the method of paralleling small-capacity fuses be used to achieve the purpose of fast fusing?
III. Questions Related to Applications
-
What design requirements for overcurrent and overvoltage protection?
-
In which fields are gas discharge tubes mainly applied? Do they have directionality?
-
Are overcurrent and overvoltage protection for AC/DC power inputs used in charging piles?
-
Can Littelfuse Circuit Protection Products Protect Against Overvoltage and Overcurrent?
-
How to specifically know the time of time-delay fusing fuses?