You may be curious about the classification terminology used for gas discharge tube surge arrestors. What do these terms mean, and how do they affect the parts’ usage?
Gas discharge tubes, often referred to as GDTs, are classified as “High voltage, low voltage; high/low surge resistance capacity”
As an example, let’s examine Littelfuse GTCS23-750M-R01-2
| DigiKey Part Number | GTCS23-750M-R01-2TR-ND |
|---|---|
| Manufacturer | Littelfuse Inc. |
| Manufacturer Product Number | GTCS23-750M-R01-2 |
| Description | GDT 75V 1KA 2 POLE SURFACE MOUNT |
| Detailed Description | Gas Discharge Tube 75 V 1000A (1kA) ±20% 2 Pole Surface Mount |
| Datasheet | Datasheet |
We can find more parameters for voltage and surge capacity in the Datasheet
The withstand voltage of GTCS23-750M-R01-2 can reach 75V DC, and impulse voltage can reach 600V (@1000 V/μs (V))
Surge Resistance Capacity:
- “8x20μs” represents the waveform of the surge current; that is, the pulse width is 8 microseconds and the pulse rise time is 20 microseconds. This waveform is a standard waveform used when testing a discharge tube’s tolerance to instant high - energy pulses.
- “1kA” means that the peak current of each pulse is 1 kiloampere. This means that the discharge tube can withstand a surge current of up to 1 kiloampere per pulse.
- “10 times” means that the discharge tube can withstand 10 such surge impacts under the above conditions (8x20μs waveform, 1kA current) without damage.
To sum up, this rating indicates that the discharge tube can withstand 10 surge current impacts of 1kA each under the 8x20μs pulse waveform.
More Littelfuse circuit protection products
Littelfuse Circuit Protection products provide stable and reliable signal transmission guarantee for all kinds of precision electronic devices by virtue of their precise adjustment relationship with capacitance, dynamic resistance, etc. in terms of high-frequency characteristics, and their performance is excellent in the industry.
More Q&A on Littelfuse Circuit Protection Products Technology:
I. Questions Related to Component Characteristics
-
Littelfuse new MOV+Sidactor thyristor vehicle charging solution technological innovations
-
In Littelfuse circuit protection products, what kind of current is I in I²t?
-
What are the differences between discharge tubes and metal oxide varistors?
II. Questions Related to Selection
-
How to select metal oxide varistors for overvoltage protection?
-
Do Littelfuse overcurrent protection fuses/circuit breakers have self-resetting function?
-
The difference in the selection of overvoltage / overcurrent between AC and DC input terminals?
-
What parameters differ between surface mount and through hole fuse selections?
-
Under what general circumstances can AC components be directly used in DC circuits?
-
Can the method of paralleling small-capacity fuses be used to achieve the purpose of fast fusing?
III. Questions Related to Applications
-
What design requirements for overcurrent and overvoltage protection?
-
In which fields are gas discharge tubes mainly applied? Do they have directionality?
-
Are overcurrent and overvoltage protection for AC/DC power inputs used in charging piles?
-
Can Littelfuse Circuit Protection Products Protect Against Overvoltage and Overcurrent?
-
How to specifically know the time of time-delay fusing fuses?