The difference in the selection of overvoltage / overcurrent between AC and DC input terminals?

Question: Are there significant differences in the selection of overvoltage and overcurrent protection components between AC input terminals and DC input terminals?

Answer: There are differences. The higher the AC or DC voltage, the greater the differences.

Regarding the differences in the selection of overvoltage and overcurrent protection devices for the input terminals of AC (alternating current) and DC (direct current) power supplies.

The protection devices involved here include Fuses Fuses, Varistors, MOVs Circuit Breakers and various other circuit protection components.

  • There are indeed differences in the selection of overvoltage and overcurrent protection devices between AC and DC. And these differences become more significant as the AC or DC voltage increases.

  • For example, in high-voltage situations, AC voltage changes periodically, and its peak voltage
    The formula for calculating peak voltage for an AC voltage value from an RMS value
    This affects the selection of overvoltage protection devices. For MOVs in AC circuits, it is necessary to consider the peak voltage the MOV can withstand and its response characteristics within the AC cycle. In DC circuits, the focus is mainly on its DC voltage withstand value.

  • For overcurrent protection, since AC current also changes periodically, it will generate reactance effects in inductors, capacitors, and other components. Taking fuses as an example, the relationship between the effective value and the peak value of AC current affects the fusing characteristics of fuses. In DC circuits, the current is relatively stable, and the main consideration is the impact of the DC current magnitude on the fuse. In high-voltage AC and DC circuits, the differences in these characteristics are more obvious, resulting in greater differences in device selection.

More Littelfuse circuit protection products

Littelfuse Circuit Protection products provide stable and reliable signal transmission guarantee for all kinds of precision electronic devices by virtue of their precise adjustment relationship with capacitance, dynamic resistance, etc. in terms of high-frequency characteristics, and their performance is excellent in the industry.

More Q&A on Littelfuse Circuit Protection Products Technology:

I. Questions Related to Component Characteristics

  1. What are the classifications of gas discharge tubes?

  2. Littelfuse new MOV+Sidactor thyristor vehicle charging solution technological innovations

  3. In Littelfuse circuit protection products, what kind of current is I in I²t?

  4. What are the differences between discharge tubes and metal oxide varistors?

II. Questions Related to Selection

  1. How to select metal oxide varistors for overvoltage protection?

  2. Do Littelfuse overcurrent protection fuses/circuit breakers have self-resetting function?

  3. The difference in the selection of overvoltage / overcurrent between AC and DC input terminals?

  4. When to Use PTC Resettable Fuses and Metal Fuses?

  5. What parameters differ between surface mount and through hole fuse selections?

  6. Under what general circumstances can AC components be directly used in DC circuits?

  7. Can the method of paralleling small-capacity fuses be used to achieve the purpose of fast fusing?

III. Questions Related to Applications

  1. What design requirements for overcurrent and overvoltage protection?

  2. In which fields are gas discharge tubes mainly applied? Do they have directionality?

  3. Are overcurrent and overvoltage protection for AC/DC power inputs used in charging piles?

  4. Can Littelfuse Circuit Protection Products Protect Against Overvoltage and Overcurrent?

  5. How to understand the fuse explosion-proof test?

  6. How to specifically know the time of time-delay fusing fuses?