I’m looking to order the good part for a CASIOPX-735 with an AC power connector 12 V AD-A12150LW.
Can you please tell me witch female socket connector jack to order? (with the positive in the center).
I’m looking for the exact DigiKey Part Number.
Would this one works? DigiKey Part Number: 2057-ADC-039-6-ND
Thank you.
Hello,
Thank you for your post.
I am not seeing a barrel diameter listed for the keyboard or the power supply. There is a very simple way to determine the inside diameter of the barrel plug. If you have a ballpoint pen, you can try inserting the writing tip of the pen into the barrel.
If the pen tip is able to fit inside the barrel then the inside diameter of the barrel is 2.5mm. If it does not fit inside then it is 2.1mm. Aside from that it could be listed in the original manual for the keyboard.