KWh meter sensors

I would like to know if the current pickup sensors are included with power meter Selec EM368-C-CU-ROHS, DigiKey part number 4106-EM368-C-CU-ROHS-ND.

If not, can I have links to current sensors compatible with this device ?

Thanks !

Hello Ybelzile,
Thank you for contacting DigiKey technical support and welcome to our community.
Our team is looking into your question.

There are a lot of current sensor tech available. I’m referring to the clamp-on-wire, transformer/coil pickup, type of sensor.

Current transformers are not included: the device is programmable to allow use of user-selected CTs suitable for their intended application. The current sense transformer family would be the place to look for such things. If the aim is to install without having to disconnect or splice into the current-carrying conductors, filtering that for the “Non-Invasive (Split Core)” type would be helpful.

Also, one would likely want to check the installation guide/instructions available from the manufacturer via this link.

All right. Thanks for answering the question. I will read the install guide.