Laser Rating for MICRO 200 from Quarton Inc

We have received a number of calls wondering what the rating is on the MICRO 200 laser from Quarton Inc. According to the manufacturer’s website the following applies to the Micro 200.

Complied with the European Standard EN 60825-1 & USA FDA Laser safety regulations.

Complied with the FDA Laser safety regulations and has Auto-Power-Control circuit which keeps the output power stable and won’t change in any temperature.

Output power: FDA Class IIIa laser, output power 1~5mW (power control under 3mW), eye safe laser product.