This article is part of a guided learning series on building and analyzing User-Defined Function Blocks (UDFBs).
Canonical Article: Building a User-Defined Function Block (UDFB) Using Siemens TIA Portal
Learning Companion (Q&A): Explore All Questions
You are reading: Question 8
The fault reset network considers both NOT xEnable and xReset as necessary conditions to perform a reset. What would happen if the NOT xEnable condition were removed. Be specific and explore this from the operator’s perspective.
Answer
This is a critical safety consideration. It prevents an unexpected and potentially dangerous restart of the motor. As written, the operator must first disable motor activation signal before attempting a reset. If the reset is successful, the operator may then restart the motors in accordance with the plant’s standard operating procedure.
Article by Aaron Dahlen, LCDR USCG (Ret.), Application Engineer at DigiKey