Learning Companion for a Ladder Logic Based User-Defined Function Block

This page contains a series of questions to accompany an article exploring ladder logic as applied to a User-Defined Function Block (UDFB) built using the Siemens TIA Portal. Please review the primary article to provide context for the following questions.

These questions may be assigned as homework, an interactive group discussion, or as part of an AI-directed learning exercise. Note that the AI can serve as a strong sounding board from which you can explore the questions.

:pushpin: Canonical Article: Building a User-Defined Function Block (UDFB) Using Siemens TIA Portal

Figure 1: Image of the Siemens S7-1200 used to develop and test the UDFB-embedded state machine code.

Recommendation for use of an AI-based More Knowledgeable Other (Vygotsky’s MKO)

This learning companion may be used as a self-guided tool with the AI serving as a sounding board. For the most effective learning:

  • Provide context for the AI by directing its attention to the canonical article.

  • Point the AI to this page and prompt it to ask each question, one at a time, from this list and provide feedback from the perspective of an experienced control system’s engineer.

  • Provide complete answers and ask for clarity where required.

Question organization in this document

Questions are listed in order of increasing complexity.

  • Explicit: The first questions are taken directly from the associated document. They are practical and directly test your understanding of the material.

  • Implicit: Questions in the middle offer increasing levels of complexity. Instead of implicitly questioning the material, they ask the reader to deeply consider the material and draw parallels to related topics.

  • Topic Adjacent: The final critical thinking question(s) address topics adjacent to the article material. These critical thinking questions expand the article’s content allowing you to develop a big picture understanding of the material and its relationship to adjacent topics. They are often open ended, require research, and are best answered in essay form.

Each question is categorized with a recommendation audience:

  • :hammer_and_wrench: Technicians – Practical, troubleshooting-oriented

  • :graduation_cap: Students – Academic understanding

  • :test_tube: Capstone students and field engineers – system-level analysis, design tradeoffs


Questions for anchored AI-assisted learning

This section contains a list of questions with answers to help you better understand the material.

:pushpin: Canonical Article: Building a User-Defined Function Block (UDFB) Using Siemens TIA Portal

1) What is a state machine? :hammer_and_wrench: :graduation_cap:

Answer

2) What are the advantages and disadvantages of each method used to hold a PLC’s state? At a minimum include the latch, set/reset coils, and numeric methods (integer state variables). :hammer_and_wrench: :graduation_cap:

Answer

3) Describe UDFB mapping and memory including input, output, static, and constant. :hammer_and_wrench: :graduation_cap:

Answer

4) Define enumeration and then describe how it assists with the design and maintenance of a state machine. :hammer_and_wrench: :graduation_cap:

Answer

5) What is the difference between an edge-triggered and a level-sensitive UDFB? :hammer_and_wrench: :graduation_cap:

Answer

6) How is PLC-based numeric state machine like a C case-switch statement? :graduation_cap:

Answer

7) Construct a graphical bubbles and arrows representation of the featured state machine. Ref: FSM State Diagrams :hammer_and_wrench: :graduation_cap:

Answer

8) The fault reset network considers both NOT xEnable and xReset as necessary conditions to perform a reset. What would happen if the NOT xEnable condition were removed. Be specific and explore this from the operator’s perspective. :graduation_cap:

Answer

9) Identify the implicit one shot in a state machine. :graduation_cap: :test_tube:

Answer

10) Select appropriate values for timGlitch and timMove in a motor starter? :graduation_cap: :test_tube:

Answer

11) What is state fall through for a state machine? :graduation_cap: :test_tube:

Answer

12) Should we use an unsigned int or type double as the state variable? :graduation_cap: :test_tube:

Answer

13) Modify the featured UDFB so that a single timer resource is used. :graduation_cap: :test_tube:

Answer

14) How to account for a motor overload. :test_tube:

Answer

15) Modify the state machine to drive a dual coil DCV. :test_tube:

Answer

16) How can a UDFB’s fault status string be used with an HMI? :test_tube:

Answer

About this author

Aaron Dahlen, LCDR USCG (Ret.), serves as an application engineer at DigiKey. He has a unique electronics and automation foundation built over a 27-year military career as a technician and engineer which was further enhanced by 12 years of teaching (interwoven). With an MSEE degree from Minnesota State University, Mankato, Dahlen has taught in an ABET-accredited EE program, served as the program coordinator for an EET program, and taught component-level repair to military electronics technicians. Dahlen has returned to his Northern Minnesota home and thoroughly enjoys researching and writing articles such as this.

LD UDFB Guided Learning Q03: – Describe UDFB mapping and memory
LD UDFB Guided Learning Q05: – Difference Between Edge-Triggered and Level-Sensitive UDFB
LD UDFB Guided Learning Q10: Select appropriate values for timGlitch and timMove in a motor starter?
LD UDFB Guided Learning Q01: – What Is a State Machine?
LD UDFB Guided Learning Q11: – What is state fall through for a state machine?
LD UDFB Guided Learning Q06: – How is PLC-based numeric state machine similar a C case-switch?
LD UDFB Guided Learning Q16: – How can a UDFB's fault status string be used with an HMI?
LD UDFB Guided Learning Q02: – Advantages of a Latch, Set Reset Coils, and Numeric Methods
LD UDFB Guided Learning Q07: – Construct bubbles and arrows representation of the state machine
LD UDFB Guided Learning Q08: – What would happen if the NOT xEnable condition were removed
LD UDFB Guided Learning Q09: – Identify the implicit one shot in a state machine
LD UDFB Guided Learning Q14: – How to account for a motor overload
LD UDFB Guided Learning Q04: – Define Enumeration as Related to a PLC-based State Machine
LD UDFB Guided Learning Q13: Modify the featured UDFB so that a single timer resource is used
LD UDFB Guided Learning Q12: Should we use unsigned int or double as the state variable?
SiemensのTIAポータルを使用したユーザー定義ファンクションブロック(UDFB)の構築
Programming Siemens GRAPH: Moore Machine Pattern
Building a State Machine in Structured Text using Siemens TIA Portal
Building a State Machine in Function Block Diagram using Siemens TIA Portal
LD UDFB Guided Learning Q15: – Modify the state machine to drive a dual-coil DCVA