Lead Indentation Marks on Vishay NTCLE203E3222SB0 NTC Thermistors

If you have observed varying degrees of indentations on the leads (as shown below) of NTCLE203E3222SB0 NTC Thermistor from Vishay
please note that we have clarified this with the manufacturer, and according to them, these indentations do not affect the functionality or reliability of the product.

Please see their response below.

The indentation detected in this lot is a tooling imprint in the wire to form the leadwires ‘bayonet’ as we call it, in order to fit the ceramic thickness in-between the two leadwires to assure that the plane of the leadwires is within certain degrees of the plane of the ceramic surface. Without it, the sensor head will mechanically turn more depending on the R-value in the NTCLE203 series.

As there are natural variations in the raw material of the leadwires, some wire lot’s have a bit more ‘spring’ effect and need to be formed more into the plastic zone, leaving more imprint of the tooling onto the leadwires.

These indentations have no effect on the functionality nor reliability of the product. These tooling imprints are imperative and will show up from time to time a bit more or a bit less.

Applicable Part Numbers
DigiKey Part Number Manufacturer Part Number
BC2298-ND NTCLE203E3103GB0
BC2299-ND NTCLE203E3103FB0
BC2530-ND NTCLE203E3473GB0
BC2446-ND NTCLE203E3103SB0
56-NTCLE203E3103FB0A-ND NTCLE203E3103FB0A
BC2300-ND NTCLE203E3104FB0
BC2728-ND NTCLE203E3272FB0
BC2461-ND NTCLE203E3502JB0
BC2460-ND NTCLE203E3474JB0
56-NTCLE203E3104HB0A-ND NTCLE203E3104HB0A
BC2447-ND NTCLE203E3104HB0
56-NTCLE203E3103GB0A-ND NTCLE203E3103GB0A
BC2457-ND NTCLE203E3472GB0
BC2730-ND NTCLE203E3302SB0
BC2732-ND NTCLE203E3502SB0
BC2452-ND NTCLE203E3202SB0
BC2456-ND NTCLE203E3472FB0
56-NTCLE203E3474JB0A-ND NTCLE203E3474JB0A
56-NTCLE203E3502JB0A-ND NTCLE203E3502JB0A
56-NTCLE203E3123HB0A-ND NTCLE203E3123HB0A
BC2450-ND NTCLE203E3202HB0
BC2444-ND NTCLE203E3103HB0
56-NTCLE203E3104GB0A-ND NTCLE203E3104GB0A
56-NTCLE203E3472GB0A-ND NTCLE203E3472GB0A
56-NTCLE203E3473GB0A-ND NTCLE203E3473GB0A
56-NTCLE203E3272GB0A-ND NTCLE203E3272GB0A
BC2529-ND NTCLE203E3104GB0
BC2731-ND NTCLE203E3303SB0
56-NTCLE203E3472FB0A-ND NTCLE203E3472FB0A
56-NTCLE203E3272FB0A-ND NTCLE203E3272FB0A
56-NTCLE203E3104FB0A-ND NTCLE203E3104FB0A
56-NTCLE203E3103HB0A-ND NTCLE203E3103HB0A
56-NTCLE203E3103JB0A-ND NTCLE203E3103JB0A
BC2445-ND NTCLE203E3103JB0
BC2448-ND NTCLE203E3123HB0
BC2729-ND NTCLE203E3222SB0
56-NTCLE203E3104JB0A-ND NTCLE203E3104JB0A
56-NTCLE203E3222JB0A-ND NTCLE203E3222JB0A
56-NTCLE203E3202JB0A-ND NTCLE203E3202JB0A
56-NTCLE203E3223JB0A-ND NTCLE203E3223JB0A
56-NTCLE203E3272JB0A-ND NTCLE203E3272JB0A
56-NTCLE203E3472JB0A-ND NTCLE203E3472JB0A
BC2449-ND NTCLE203E3123JB0
BC2451-ND NTCLE203E3202JB0
BC2454-ND NTCLE203E3272JB0
NTCLE203E3104JB0-ND NTCLE203E3104JB0
NTCLE203E3472JB0-ND NTCLE203E3472JB0
NTCLE203E3473JB0-ND NTCLE203E3473JB0
56-NTCLE203E3683JB0A-ND NTCLE203E3683JB0A
56-NTCLE203E3473JB0A-ND NTCLE203E3473JB0A
56-NTCLE203E3123JB0A-ND NTCLE203E3123JB0A
56-NTCLE203E3473HB0A-ND NTCLE203E3473HB0A
56-NTCLE203E3474HB0A-ND NTCLE203E3474HB0A
56-NTCLE203E3502HB0A-ND NTCLE203E3502HB0A
56-NTCLE203E3683HB0A-ND NTCLE203E3683HB0A
56-NTCLE203E3223HB0A-ND NTCLE203E3223HB0A
56-NTCLE203E3222HB0A-ND NTCLE203E3222HB0A
56-NTCLE203E3202HB0A-ND NTCLE203E3202HB0A
56-NTCLE203E3472HB0A-ND NTCLE203E3472HB0A
56-NTCLE203E3272HB0A-ND NTCLE203E3272HB0A
BC2459-ND NTCLE203E3474HB0
NTCLE203E3272HB0-ND NTCLE203E3272HB0
NTCLE203E3473HB0-ND NTCLE203E3473HB0
56-NTCLE203E3683GB0A-ND NTCLE203E3683GB0A
56-NTCLE203E3502GB0A-ND NTCLE203E3502GB0A
56-NTCLE203E3474GB0A-ND NTCLE203E3474GB0A
56-NTCLE203E3202GB0A-ND NTCLE203E3202GB0A
56-NTCLE203E3222GB0A-ND NTCLE203E3222GB0A
56-NTCLE203E3223GB0A-ND NTCLE203E3223GB0A
56-NTCLE203E3123GB0A-ND NTCLE203E3123GB0A
BC2453-ND NTCLE203E3272GB0
BC2458-ND NTCLE203E3474GB0
NTCLE203E3502GB0-ND NTCLE203E3502GB0
BC2455-ND NTCLE203E3272SB0
56-NTCLE203E3103SB0A-ND NTCLE203E3103SB0A
56-NTCLE203E3302SB0A-ND NTCLE203E3302SB0A
56-NTCLE203E3202SB0A-ND NTCLE203E3202SB0A
56-NTCLE203E3502FB0A-ND NTCLE203E3502FB0A
56-NTCLE203E3222FB0A-ND NTCLE203E3222FB0A
56-NTCLE203E3473FB0A-ND NTCLE203E3473FB0A
56-NTCLE203E3202FB0A-ND NTCLE203E3202FB0A
NTCLE203E3202FB0-ND NTCLE203E3202FB0
NTCLE203E3473FB0-ND NTCLE203E3473FB0
NTCLE203E3502FB0-ND NTCLE203E3502FB0