------Question for APC-8-250 Please Put your question below------
Hello,
I need to replace the current LED strip (which are COB 2835, with 150 led/m, 1 cm large) with a new one, which should fit in the existing lamp (outdoor).
Which strip (brand/model) do you recommend to buy keeping the same specs, to be driven by the APC-8-250 driver?
Thanks,
kind regards,
Giulio
Greetings,
Compatibility of an LED device with a given driver depends mostly on two things:
-
The LED device having a rated maximum current equal or greater than the driver’s rated current output (250mA for the driver in question)
-
The LED device having a forward voltage within the driver’s specified range.

Selection criteria after this may include physical form factor/size, color temperature, and CRI. These are the current listings in stock which would appear to most closely match your interests. Please note though, that commercial lighting fixtures often use custom LED arrays rather than off-the-shelf modules, so there is a strong possibility that there will be no direct replacement available in the retail market.