Looking for a cable for Laird FG9026

Hello I was looking to source a cable LMR-400 equivalent or better with terminations of N Type male on one end and a RP-SMA male on the other. In the length of around 5m (16ft) and/or 7.6m (25ft) or maybe even 15m (50ft). Do you offer such products?

It is to connect the Laird FG9026 (https://www.digikey.ca/en/products/detail/laird-connectivity-inc./FG9026/2392197) to a helium miner (SenseCAP M1 LoRaWAN Indoor Gateway - US915 - Seeed Studio).

Thank you for any help.

Hello User48,

Welcome to the DigiKey TechForum.

I was able to find 3608-WF6008-ND

Please note this part is a marketplace part, we do not stock this and once placed on order it will ship from the supplier.

However this is the 1.8m or 6ft length version. Unfortunately we have nothing longer with both N type on one side and RP-SMA on the other.

In the link

you’re able to filter by 1st connector and second connector or by style, cable length and type, etc.

Hope that helped somewhat.
Thanks for choosing DigiKey and have a wonderful day.

1 Like

Thank you for your help.